(0)| 2/27/2011 6:07 PM | |
|
Posts: 2964 Rating:
|
Hello, Looks like the password level is not there that why it showing access deined...... USER_CLASS_READ_PROGRAM - 0 USER_CLASS_WRITE_PROGRAM - 7 USER_CLASS_SELECT_PROGRAM - 7 With the above mentioned changes in the Display MD we will not be able to Create or Open or Copy or Delete any part programs. However we can Rename an existing program as well as Execute the existing part program in AUTO Mode. Note: Ø The above mentioned procedure is applicable for all the Access Levels i.e. § User Level Access.§ Manufacturer Level Access§ Expert Level AccessØ If any corrections / modifications are to be made in the part program, the same could be done by using correct program option in AUTO Mode. Check this PDF doc may be useful.... Regards, Ekalavya AttachmentChanging access authorization levels for programs.pdf (212 Downloads) |
Follow us on