(0)| 2/26/2011 10:17 AM | |
|
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hi AR, You have to Define only 1 SPOSA application Satation & Define the Client path in that. & you need to download in to the Client PC. & have to transfer the OpenPCS7 License on the Client PC. then Open the OPC Sout V10 & cheked the OPC are connected or not. here is the Example Link & Steps here is the Manual seethe Chapter 4.1 Configuring an OpenPCS 7 station |
Last edited by: Ammy at: 2/26/2011 10:25 AMAmmy |
|
Follow us on