3/13/2011 9:58 AM | |
Posts: 2964 Rating:
|
Hi, Lubrication is controlled according a specified time interval for a specified duration (not distance related). A manual key is available to start lubricating, and during power on of the machine tool it is also possible to start lubrication. Normally the lubrication will be started periodically in the time interval defined by input parameter Lintv. The lubrication lasts for the duration specified by another input parameter Ltime. In case of emergency stop, lubrication motor overload, lubrication will be not started. 2 alarms will be activated in this subroutine: Alarm 700020 – LUBRICATING MOTOR OVERLOAD Alarm 700021 – LUBRICANT LEVEL LOW MD 14510 [24]: Lubrication time interval (unit: 1 min) MD 14510 [25]: Lubrication duration (unit: 0,01 s, max. 327.67s) Check this pdf document for further more informations Regards, Ekalavya AttachmentPLC_appl_Program.pdf (405 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on