(0)| 11/5/2010 8:48 PM | |
|
Posts: 1742 Rating:
|
Hello, It is hard to find back from the BIB number what block you mean. If you could post a screenshot of the block call, it could be helpfull. |
| 11/9/2010 12:53 AM | |
|
Joined: 10/7/2005 Last visit: 1/12/2026 Posts: 3054 Rating:
|
It does dear PLC9, it means that it isa Siemens "Standard" FB's which could bemathematical, comms related DHB's, IP cardrelated etc. etc. etc. (you'll find for example the manuals - and BIB numbers - forthe basic "standard" FB's HERE and mathematical "standard" FB's HERE, but there's heaps more "standard" FB's available depending on the type of S5CPU's and/or IP/CP that is used) Giving us the information thatjklmasked for would certainly help us being able to advise you and please let us also know what S5 CPU it is and what "function" it is meant to fulfill. I hope this helps |
|
Cheers |
|
| 11/16/2010 10:13 AM | |
|
Posts: 5 Rating:
|
Thanks for your reply, jklm. To convert GRAPH i have this program: G5KONVNT. The problem about FB 70 i`m trying to solve it. Best regards, |
Follow us on