4/1/2011 10:05 AM | |
Posts: 2 Rating:
|
Hi i am looking for any one who ca assist me with 2 question i have regarding the communication of S5. Question 1 I have a S5 CPU 98B with a SINEC L2 6GK1543_1AA01 comms card. The CPU is talking to a PC that has Wonderware V6b. The client wants to upgrade to a higher version preferably Wonderware Intouch V10, but the L2 card in the PC is only supported by lower operating systems.(95/NT) Were as Intouch V10 needs Windows XP. My question is if I can keep the SINEC L2 6GK1543_1AA01 on the plc but change the CP Card on the PC. What CP card will be compatible to use so I can run Windows XP and Intouch 10 and the SINEC L2 6GK1543_1AA01. [schnippschnapp]second question is splitted to communication between CPU 98B and PC using com port1. |
Last edited by: O_Moderator at: 4/1/2011 10:22 AM |
|
Follow us on