(0)| 4/2/2011 4:41 PM | |
|
Posts: 3 Rating:
|
Dear all, I use PCS7 Ver 6.1, For the first, i have tried GSD file upgrade (2BA02) but it shows error for step7 ver5.3.. So i install Step 7 ver 5.4 to configure im153-2 (2BA02)hardware..I just use profibus Dp connection...Of course it work well when using PLC but when i used PCS7 (CFC + SFC), i'm facing a lot problem with my software...DO signal cannot been produce...Is there any solution for this...is it by upgrading PCS7 version by using Ver 7 is the only way....?? rgds RUKU Splitted from GSD-file for 6ES7-153-2BA02-0XB0. |
Last edited by: O_Moderator at: 4/5/2011 10:03 AMnew subject after splitting |
|
| 4/2/2011 4:56 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, OFFTOPIC Is not recommended to update Step7 version in case of PCS7. The rule there is to update PCS7 using corresponding SPs or updates. The second point is to take in mind PCS 7 V6.1 Released Modules. (for example). Each version of PCS7 has its corresponding released modules. Of course is possible to install GSD file but after you should manual prepare the software. Best regards, Hristo Mihalev |
This contribution was helpful to
|
|
| 4/6/2011 1:51 AM | |
|
Posts: 2661 Rating:
|
The upgrades should be done (when permitted) using the so-called HSP's (Hardware Support Package) for example: HSP for ES integration of Standard ASs with CPU V5 in SIMATIC PCS 7 V6.1 + SP1 Also, what exactly is the problem? You have new spare modules that have a newer order number? If that is the case you can configure BA00 in HW config and actually plug-in BA02 in the field. Regards |
Follow us on