4/8/2011 10:57 AM | |
Joined: 10/3/2010 Last visit: 6/14/2024 Posts: 1552 Rating: (188) |
things work fine, I adjusted a few things regarding my needs (like the 2 bits are replaced by properties instead of internal tags),... Your input is a much better help for understanding faceplates than the manuals Thanks once again |
B r g d s , |
|
4/8/2011 6:28 PM | |
Posts: 291 Rating: (68) |
Thanks a lot ~ SteBo!! Thanks for testing the faceplate & telling me it works!! Have a nice weekend,
Komi |
4/14/2011 1:17 PM | |
Joined: 10/3/2010 Last visit: 6/14/2024 Posts: 1552 Rating: (188) |
Hey Komi, I've used and changed one of your faceplate examples. Things work pretty except when the external tag value is 0, the color animation of the bits on the faceplate instances is not executed whenever opening the picture containing the faceplate instances. Could you please check this? Thanks in advance. best regards, SteBo Attachment16Bit_Display.zip (536 Downloads) |
Last edited by: SteBo at: 4/14/2011 1:33 PMMeanwhile, I solved this by putting a default input value "-1" see updated attachment B r g d s , |
|
Follow us on