(1)| 5/18/2011 10:00 AM | |
|
Joined: 12/18/2006 Last visit: 10/22/2025 Posts: 89 Rating:
|
Hey It seems that still on rack-pc 547B you cannot use the CAS recovery DVD. Using that I did not get the shared folder \\CAS\Archivedir\. Can someone tell me if I can manually share some existing folder and will it be enough to get CAS to work or do I have to recover a clean Win2003 and install CAS from the PCS7 DVD (v7.1+SP1)? Splitted from Central Archive Server / StoragePlus notes. |
Last edited by: O_Moderator at: 5/19/2011 10:37 AMnew subject after splitting |
|
| 5/18/2011 7:23 PM | |
|
Posts: 385 Rating:
|
Hey Skata, It is recommendable to new install CAS from the PCS 7 DVD V7.1 SP1 on Windows Server 2003 SP2. Regards |
Last edited by: JOTST at: 5/18/2011 7:24 PM |
|
Follow us on