(0)| 6/20/2011 10:22 AM | |
|
Joined: 9/18/2006 Last visit: 12/8/2025 Posts: 596 Rating:
|
Hi. From the PLC (V28001010.0 = 1) output (DO9) is set? If the output (DO9) from the PLC is setting, you can choose to set the signals: V28001009.0 or V28001011.0 or V29001004.0 I can not verify. Best regards. AttachmentSignals to fast inputs and outputs.pdf (200 Downloads) |
Last edited by: pfuser at: 6/20/2011 10:31 AM |
|
Follow us on