(0)| 8/18/2011 3:35 PM | |
|
Posts: 4 Rating:
|
I do also have a problem on our set-up here, we are on the commissioning period. We are using a 3rd party software to communicate or get the DA, HDA and AE data. DA and HDA are doing well but the AE, our OPC Client was unable to extract data from the WINCC OPC Server. By the way we are using Knowledge Manager from ABB and our Server WINCC is version 6.0 then connectivity pack was installed also to make it work.Our set-up is, we installed connectivity pack bothon our OS Server and OS Client then our 3rd party software extracts data thru OS Client. Is this correct? Is there some other possible way to extract the AE data or is there any tool to test it? Splitted from opc client connection. |
Last edited by: O_Moderator at: 8/19/2011 12:00 PMnew subject after splitting Last edited by: O_Moderator at: 8/18/2011 8:08 PMcontact data deleted |
|
Follow us on