(0)| 8/26/2011 1:28 PM | |
|
Posts: 96 Rating:
|
Hialexpozharov, I think it is not the function., it is your object were the Block comment is written (normally a text field). Check the property of the field may be it is setup to blink. If I want to make a new/customised faceplate then I normally copy some standard faceplate and modify it because in that way you don't have to worry about the standard function. You might get some errors when you are saving the faceplate because some of the object might be accessing other objects which you might have deleted. A message will be displayed when you save which will direct you to the file containning the details of the error. It is simple and I think you can solve it easily. Hope this was useful. Regards, mk
|
Follow us on