(0)| 10/18/2011 11:48 AM | |
|
Posts: 3037 Rating:
|
Hello, You can display the process variable in the trend or you can display archive variable in the trend.You may logging process variables. Then you must create a data log. Now you add the variable to this data log. See the manual at page 63.WinCC flexible Getting Started Power User
1. In this case you must just the trigger “On demand” for logging. This trigger is described in the following manual at page 284.WinCCfelxible manual 2. At this FAQ can you see how you can display the process variable in a CSV file. How can you output batch data or archived data via an HMI operator panel? 3. You must use the function “ ArchiveLogFile”. With this function can you copy the logfile. For thisfunction you must use data log with logging method “ Create segmental circular logs automatically”. 4. You must calculate the size of the log. This is described in the manual on page 282.WinCCfelxible manual Here is some information for logging in the following FAQs. How are tags and alarms logged in WinCC flexible?How do you do long-term archiving with WinCC flexible? WinCCfelxible manual |
Follow us on