(0)| 10/19/2011 9:16 AM | |
|
Posts: 20 Rating:
|
Dear all, I am using CPU-315-2PN/DP withET-200S IM-151-3PN I Have Connected The encoder as per the ET 200 s Technological functions manual attached herewith Terminal Module TM-E30S-44-10 Page no- 123, also the program made as per the referenceprg in the manual page no 121.Attachedfiles contain encoder of 5v to 24v manual and ET200S manual. I am getting the status bit with error ERR_ENCODER continusly ONand so i cant read pulses.how can i make it healthy. .Please Help me. prg sample... Block: FC101 Network 1: Presettings L 0 //Delete control bits T DB1.DBD0 T DB1.DBD4 SET S DB1.DBX4.0 //Open SW gate Network 2: Write to the control interface
T PAD 256 //Configured start address of the outputs L DB1.DBD4 T PAD 260
//Read 8 bytes from the 1Count5V/500kHz
T DB1.DBD8 L PED 260 T DB1.DBD12 Attachmentdatasheet.pdf (404 Downloads) |
Follow us on