(0)| 11/14/2011 10:29 PM | |
|
Posts: 11 Rating:
|
Hello everyone I´ve had a big problem adding some instruments (Endress Houser) to an existant project. I have added the corresponding EDD files to the system through the tool"Manage Device Catalog" from PDM, however once I want to use them in the HW Config to add them in the corresponding Profibus PA Network, they are not in the Catalog, simply I can not find them, I already look for them in some other folders but they are not listed. When adding in the Manage Device Catalog, no error ocurres and if doing it again the system says they are already in the system. For me, it may has to do with the version of the PDM, probably the instruments are too new for my PDM version; but I´m not sure. Any idea ?? Any suggestion will be helpful Note. When trying to update the Hardware Catalog, I found a log with an error that may help (attachment). Product: SIMATIC PDM Version: V6.0 + SP1 + HF3 Release: K06.00.01.03_01.01.00.02 Release number: K06.00.01.03 Saludos! Ricardo Ibáñez
AttachmentUpdate_error_111111.zip (307 Downloads) |
Follow us on