(0)| 11/23/2011 2:19 PM | |
|
Joined: 9/19/2011 Last visit: 1/6/2026 Posts: 141 Rating:
|
What version of firmware do you have in the 231-5QD30 module? If you do not have V01.00.05 then see this link to upgrade. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&nodeid0=41886031&nav0=tree&lang=en&siteid=csius&aktprim=0&extranet=standard&viewreg=WW&objid=41885258&treeLang=en This should fix the problem that you are seeing. |
| 11/23/2011 6:06 PM | |
|
Posts: 1 Rating:
|
make sure that you ground the module and connect the M of the 24V Supply to the same ground instruction sheet for module should provide additional details |
| 11/24/2011 1:09 PM | |
|
Posts: 1410 Rating:
|
Have you measured TCs too see if they are floating type or they are grounded? |
Follow us on