(0)| 12/16/2011 8:57 PM | |
|
Posts: 8946 Rating:
|
Dear Sparrow, the TP177B support recipes without optional Add-On. My idea is, to export and import recipes (funtion is already included in panel) onto an existing net-path via UNC. (i.e. \\MyServer\Recipes). The path for all panels must be the same. So panel 1 do export recipes that will be imported from panel 2 and vice versa. It works pretty good with WinCCflex RT on PC and should work also with a TP177B. If it is possible with an TP177A, I am not sure. "the same Ethernet network where the two TPs and the Runtime-PC will be connected?" Yes. Best regards Jürgen. |
| 12/18/2011 10:55 PM | |
|
Posts: 8946 Rating:
|
UNC-Path: http://en.wikipedia.org/wiki/Path_(computing) "\\ComputerName\SharedFolder\Resource " |
| 12/19/2011 9:58 AM | |
|
Joined: 4/24/2006 Last visit: 12/24/2025 Posts: 9097 Rating:
|
Dear Sparrow, Some additional information. Perhaps this link is useful: WinCC flexible: Engineering with Recipes Using Integrated Functionalities When you use WinCC flexible RT, you will need additional licence when using recipes!! Best regards, Wizard |
Follow us on