(0)| 1/20/2012 10:08 AM | |
|
Posts: 836 Rating:
|
Hi, PCS 7 6.1 SP3 is using WinCC 6.0 SP3 (a + HF24). For WinCC 6.0 SP3 you have to use WinCC/Connectivity Pack V6.1 (according to Compatibility Tool). First I was looking up the Compatibility with PCS 7 and WinCC and then the compatibility with WinCC and Connectivity pack. But: There is no direct compatibilty between PCS 7 and Connectivity Pack listed. This means that this was not tested. Because PCS 7 is always a little bit different that native WinCC, there could be problems. But it could also work without problems. Check out this FAQ and the linked Compatibility Tool to see wich product are compatible with wich PCS 7 version: http://support.automation.siemens.com/WW/view/en/2334224 Check out this FAQ to see compatibility for WinCC: http://support.automation.siemens.com/WW/view/en/49382338 |
Last edited by: Silent Bob at: 1/20/2012 10:15 AM |
|
| 1/23/2012 1:16 PM | |
|
Posts: 836 Rating:
|
Hence all Versions of PCS 7 6.1 are using the same WinCC (6.0 SP3), I would say that Connectivity Pack v6.1 is compatible for all service packs. |
| 1/23/2012 4:34 PM | |
|
Posts: 160 Rating:
|
Hi Silent Bob, You have good point. Thanks |
Follow us on