(0)| 2/9/2012 10:24 AM | |
|
Posts: 206 Rating:
|
Hello GOCHEV, you can´t use the 7MH4607-8CA cable for Siwarex FTC. The reason is that the Siwarex FTC has a 9 pin d-sub connector to Siwatool and the 7MH4607-8CA cable has open wires for connection to Siwarex U. So only the cables 7MH4702-8CA (2m) or 7MH4702-8CB (5m) will work. Look also in the manual chapter 4.4.13 http://support.automation.siemens.com/WW/view/en/20072206 Regards ABenno |
| 2/9/2012 3:56 PM | |
|
Posts: 9 Rating:
|
thank you very much , ABenno! |
Follow us on