(2)| 3/8/2012 8:41 PM | |
|
Posts: 25 Rating:
|
Hi Hosseini, Thanks, I already checked my program, there are SFC14 and SFC 15 also SFB 14 and SFB 15 but inside of them there is nothing they are blank. Rahul |
| 3/9/2012 1:10 AM | |
|
Joined: 1/28/2009 Last visit: 1/5/2026 Posts: 6892 Rating:
|
Dear Sir, There is no thing useful inside SFC15 for us to investigate. Find the place SFC15 is called,Check the address for "Record" parameter.It would be like this: P#DB13.DBX0.0 byte 10 Find the address with the determined length and see how the programmer packed data in the memory area! Also refer to this tip: Please upload the source project or snapshots related to your question
Best regards, Hamid Hosseini AttachmentSFC15.pdf (321 Downloads) |
| 3/12/2012 7:57 AM | |
|
Joined: 10/7/2005 Last visit: 1/18/2026 Posts: 3054 Rating:
|
Hello RahulSharma unless I missed something, the answer to your above question is in your screendump of your intitial post and attached is an annotated copy of it which hopefully helps. |
|
Cheers |
|
Follow us on