(0)| 3/20/2012 10:03 PM | |
|
Posts: 20 Rating:
|
Thanks Silent Bob, I thought as much that I would have to use another associated-value for the limits, just hoped there was a another way. Thanks again Cammo
|
| 3/23/2012 12:52 PM | |
|
Posts: 836 Rating:
|
Hi Cammo, check out this FAQ. Maybe you can create your message text in a string and connect it to one associated value. http://support.automation.siemens.com/WW/view/de/674578 |
Last edited by: Silent Bob at: 3/23/2012 12:52 PM |
|
| 3/27/2012 6:31 PM | |
|
Posts: 170 Rating:
|
Another possibility is the use of an User Text Library. I have already built an User Text Library for the current APL Engineering Units cross reference to text (attached Library Archive File, APL_EUs_TextLib).Just copy paste from thisarchived libaray (after retreiving) to the program folder of an AS project where required. To use the text library just connect the enumerated value (not structure) of the engineering units to an available aux value/ext value. In the Event text of a message you enter the typical placeholder for aux val/ext values but include the text library as the format (%t#<Name of Text Library>) being used, i.e. @5I%t#APL_EUs@. AttachmentAPL_EUs_TextLib.zip (194 Downloads) |
Follow us on