(0)| 3/27/2012 9:46 PM | |
|
Joined: 7/17/2010 Last visit: 11/12/2025 Posts: 189 Rating:
|
Personnel. I am creating a log with the date 1200 and I am with some doubts about the program, I used an example that the siemens site to create a log link and this example: https://www.automation.siemens.com/BR/tf/WW/en/Posts/57715#top Until then I'm in doubt as to the operation of the memories that are described in the program. And another doubt I have to create a loger two analog readings I'm using a function Norm X to input two analog sensors, my doubts too, and how I should address the analog values read by the Log Data to create history. See the attached program Attachmentprogram.zip (565 Downloads) |
| 3/28/2012 12:24 PM | |
|
Joined: 9/23/2005 Last visit: 1/15/2026 Posts: 4447 Rating:
|
Hi, About the "Sample program: S7-1200 and DATA LOG" I'm not sure what type of information do you ask. Can you explain? In then refered link, at 2/13/2012, 10:53 AM , I post a cast, where I show how to operate the example. About the analogic variables: I'm also not sure about your doubts. Can you explain? You can place the analogica value directly (e.g. from 0 to 27648) or converted (there is a sample program in FAQ /tf/WW/en/Posts/31698#top |
|
Denilson Pegaia |
|
Follow us on