(0)| 4/23/2012 1:33 PM | |
|
Posts: 3037 Rating:
|
Hello, you can use address or tag multiplexing in WinCC flexible. How does address multiplexing work? How does tag multiplexing work? Tweety |
| 4/23/2012 1:46 PM | |
|
Joined: 9/28/2005 Last visit: 12/9/2025 Posts: 2957 Rating:
|
I suppose we speak about S7-1200. Well if project is integrated then you can use for sure the tags without absolute address. If projects are separate then I don't even know how it would be. I think you can't acces it. Its the same as it was back in 10.5 where you need to unchech 'Symbolic access only'. So maybe its a good idea to keep one block for communication with Flexible as S7-300/400 compatible. Here is the link about 10.5 How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2? It was called 'symbolic access' back then, but I think its the same thing as 'optimized' access in TIA V11. Also this link could be interesting Which system properties should you pay attention to in selecting the block access for an S7-1200 CPU when creating a new FB in STEP 7 V11? |
Last edited by: Darius at: 4/23/2012 1:47 PMBest regards, |
|
Follow us on