(0)| 4/24/2012 1:41 PM | |||||
|
Joined: 2/16/2011 Last visit: 4/28/2025 Posts: 229 Rating:
|
Dear, It depends of CPU model. See LinkS7-1214. In S7-1214 case, it have 50Kbytes of work memory, see section "CPU Blocks"
But the CPU has 2Mb of Load Memory, if you can, you can modify the atribute of the DB to "only Store in Load Memory" and use the apropriate SFC's to Read and write some bytes. In Load memory the DB can be larger but the acess is throw SFC's. Reagrds
|
||||
|
Gabriel de Oliveira |
|||||
Follow us on