(0)| 4/24/2012 4:39 PM | |
|
Posts: 1 Rating:
|
Another way if you have the program and a CF card reader then you can use the "Load to files system". Right click on the D425 controller and look for load to file system and select you CF card and it will create or write over the current user directory. Note: If the user directory is the only driectory on the card then you have to load the firmware that can be downloaded on the Siemens web site here -https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=31045047&caller=view Unzip the downloaded firmware and copy it to your card. This will create a card that the simotion controller can use.
|
Follow us on