(0)| 3/17/2012 4:46 PM | |
|
Posts: 3 Rating:
|
hello, Is there any way to resize a fceplate during runtimeby grabbing the mouse to the required size. Thnks. |
| 3/19/2012 5:35 PM | |
|
Posts: 1 Rating:
|
I think that it is not possible to do that in Runtime, only in WinCC Graphics Designer. As shown on the figure attached. |
| 4/26/2012 1:14 PM | |
|
Joined: 10/26/2011 Last visit: 1/13/2026 Posts: 766 Rating:
|
Hello How Guilherme Fuzato said, a resize of faceplates in runtime is not possible. I don't know any requestof any customer to have this functionality. Do you wantlarger or smaller faceplates? What is the reason to have this resize function? However, with WinCC Graphics Designer you can make everthinglarger or smaller, but that will be not longer PCS 7 standard. If you update your PCS 7 version, you have to look for your changes. Regards |
Last edited by: Thunderstorm at: 4/26/2012 1:30 PMSIMATIC PCS 7 - Overview |
|
| 4/26/2012 4:38 PM | |
|
Posts: 215 Rating:
|
Hi E@K, Can you elaborate more about why you have this kind of requirement? |
| 4/27/2012 12:35 AM | |
|
Joined: 11/4/2011 Last visit: 1/12/2026 Posts: 256 Rating:
|
Guilherme Fuzato, you should've mentioned that you are showing how to resize a Block Icon but not the faceplate. E@K, if you want resize the faceplate you must find out where the property Miscellaneous - Sizeable is set to YES in some Picture Window. For example, open @PG_<blockname>.PDL, select Picture Window named View, put Sizeable property to YES. Save pdl, look at faceplate in Runtime - now you can change the size just of the View window. I guess, you need to change this property in the main Picture Windows, where our faceplates are opened. They are located at @1001.pdl and their names are @TOP09, @TOP10 etc. But you can not just make Sizeable=YES there, because this setting is changing somewhere else in the scripts during compilation, I guess... For example, we would resize Message or a Memo View to see more information |
Last edited by: TerminalBuzz at: 4/27/2012 8:49 AMtrifles |
|
Follow us on