(1)| 5/20/2012 3:45 PM | |
|
Joined: 11/4/2011 Last visit: 1/12/2026 Posts: 256 Rating:
|
Hi Saravana kumar, you meant FB 1001 C_DRV_1D (not U_DRV_1D) right? I guess you have a wrong FBs structure around your motor's blocks. Have you looked at the example project of CEMAT? Open AS1 project and CFC 312_SC1 there. You see M01 motor (Screw Conveyor 2) of type C_DRV_1D. Right click on ESVG input => Jump back. Now you see M01_ESVG1 block of type C_INTER5 and two blocks of type C_ANNUNC, which are generating messages for M01 motor. Their names begin with "M01" ‒ this is very important. It gives a possibility to assign their messages to M01 motor. Try to do the same And read about this trick here: How can you display the messages of another block in addition in a PCS 7 faceplate? I hope this is it, but not shure because in C_INTER5 the "Origin" field seems to be "$$AKZ$$".. |
Follow us on