4/5/2007 1:37 PM | |
Posts: 5822 Rating:
|
Hello, could you please post a Screenshot of the PG/PC Interface Settings of your used CP? This would help me to understand. Best regards J_Bell |
4/5/2007 2:42 PM | |
Posts: 7 Rating:
|
J_Bell, I have uploaded the settings image. I have been in touch with Siemens directly & have tried every suggestion they made. I even tried restoring a backup image of the PG. This allowed me to go online once & then after that I got the 'Incorrect Highest Node Address' error again?. I am connecting to the CPU MPI port via a piggy back connector for Profibus. I will try after the bank holiday to connect directly to the MPI port although Siemens say the Profibus settings should not effect the MPI settings. I really don't get this problem as the hardware and projects have not changed & getting online previously was no problem. Regards Paul. |
4/5/2007 3:46 PM | |
Posts: 7 Rating:
|
J_Bell, Already tried both CP 5611 (Auto) & PG/PC is the only master on the bus. The Network Search returned the bus parameters in the attached image. Thanks Paul. |
Follow us on