(2)| 7/20/2012 7:48 AM | |
|
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, To make a backup off the program: 1. make sure you can connect to CPU, check settings in PG/pc interface. 2. make a new empty project and select in the TAB PLC upload station, follow the messages on the screen. You now have the program and hardware config on your PC, but there are no symbols, comments and variable names in it, so hard to read. Better get the original program from writer. The firmware can be read in the Hardware Config. I have attached a few pictures to show. About that CP-413, can you give us the 6ES7.... number written on it? Regards, Marcjan Attachmentfirmware.pdf (556 Downloads) |
Last edited by: Marcjan at: 7/20/2012 8:03 AMProblem solved? |
|
Follow us on