(0)| 6/21/2012 10:28 PM | |
|
Posts: 12 Rating:
|
I' ve a problem in START Sinumerik 880T GA2. When, Power-up the control diagnostic on operator panel, appears on the screen the diagnostic display an error in application BAS-DIO (yellow highlight) The LEDs on the CPU in the operator panel (OP CPU) the four LEDs flashing simultaneously on the operator panel. In Board INT-KEYBORD the led is yellow highlight In board PLC-CPU the led is on In board INT/DMP the led in on I chance the OP-CPU (6SN1120-4BD03) on operator panel. I check the connection between the operator panel and NC (check de cable) I chance power supply in OP and NC the error in application BAS-DIO is present. Can someone help me? AttachmentDoc2.pdf (193 Downloads) |
| 7/21/2012 10:15 PM | |
|
Joined: 7/7/2011 Last visit: 1/12/2026 Posts: 92 Rating:
|
did you initalise the com card on the rear of the monitor? you use the rotary switch on the back |
Follow us on