4/9/2007 4:51 PM | |
Posts: 9 Rating:
|
Hi Late: Tanks’ for your answer. There are two production lines, almost the same configuration but the same function. Each one has two Controllers on different Rack. These are some hardware contained in controllers of one system. DRIVES PLC:CPU 948,CP 523,IP 246,524, CP 143, IP 240,IM 308C, PROCESS PLC: CPU 948,CP 523, CP 524, CP 143, IP 240, IM 308C, I hope you can advise me about the best option for the migration.Best regards. AttachmentmS5toS7 2.zip (593 Downloads) |
Follow us on