(2)| 8/3/2012 9:07 AM | |
|
Joined: 2/20/2012 Last visit: 4/23/2018 Posts: 11 Rating:
|
Hi Sören, there are several options for accessing a PCS 7 system from outside. 1. OS Web option Access to the OS servers via a browser through installing a web server. Problem here is, only Internet Explorer is released (for versions see SIMATIC Process Control System PCS7 Web Option for OS (V8.0) http://support.automation.siemens.com/WW/view/en/61187433). 2. RDP access as you described I think this is a critical solution because you would have to configure all the security aspects on your own. You would also have to check all the systems in between your local and the remote machine. 3.SIMATIC Remote SupportService with the common Remote Service Platform Have a look at http://support.automation.siemens.com/WW/view/en/42346681. There you will find a very good option for accessing your PCS 7 system remotely via a secure connection with varying options for users, rights, accessible systems etc. In my opinion this is a very good solution. Regards, Alex |
|
Gruß / Regards, |
|
This contribution was helpful to
|
|
Follow us on