(0)| 8/2/2012 4:08 PM | |
|
Posts: 3037 Rating:
|
Hello, You can use the following link for OPC communication with WinCC flexible. You can find the configuration of DCOM interface in attachment 1. Which settings are required in Windows XP SP2 and WinCC flexible for server-client communication via OPC-DCOM? Tweety |
| 8/3/2012 1:01 PM | |
|
Posts: 3037 Rating:
|
Hello, Do you use theprojects on the following link? Which settings are required in Windows XP SP2 and WinCC flexible for server-client communication via OPC-DCOM? You should use these project for a function test. You disable the firewall on your two computer. Does the communication of server-client work? Tweety |
| 8/4/2012 7:43 AM | |
|
Posts: 119 Rating:
|
yes i have use the projects of following link ,and the communication has been develop between server and client ,but not acessing tags of server PC |
| 8/6/2012 1:55 PM | |
|
Posts: 3037 Rating:
|
Hello, You have not the right configuration of the DCOM interface. See in the following link the part 0x80070005 (DCOM ACCESS_DENIED). This is your error inyourlast screenshot. http://technet.microsoft.com/en-us/library/ee692772.aspx Tweety |
Last edited by: Tweety at: 8/6/2012 1:56 PM |
|
Follow us on