(0)| 8/13/2012 5:37 AM | |
|
Joined: 6/20/2008 Last visit: 9/21/2025 Posts: 79 Rating:
|
Hi everyone, Currently we must integrate one RED670 relay into SicamPas V5.11 SP5 system but I have not had any experience about commissioning or setting for RED670 rerlay before. So could you give me an idea about this. Now i only have PCM600 V1.5 SP2 Engineering (not Engineering Pro), so maybe i only can read and parameter the setting for this relay, cannot commission IEC61850 for the relay. Please confirm me the below step is right for integrating this relay in to SicamPas V5.11 SP5? + Step 1: Read the setting from the relay + Step 2: Export the .CID file from PCM600 (right click to the IED) + Step 3: Open a new project in CCT + Step 4: Import the above .CID file + Step 5: Do commissioning IEC61850 protocol for this relay + Step6: Export to .ICD file and - Import again .ICD file to PCM600 and download setting to the relay - Import this .ICD file to SicamPAS V5.11 SP5 (fullserver) to connect the relay into the system But now i have only the setting file of RED670, i don't have CCT tool. So could some can help me to add some information to the dataset in CCT and send the ICD file to me? Because it's so urgent, so pls help and reply me as soon as possible? Regards, NTV AttachmentF87L.zip (644 Downloads) |
| 8/24/2012 3:03 PM | |
|
Joined: 10/9/2007 Last visit: 1/16/2026 Posts: 1295 Rating:
|
Hi ABB can help you better in this case. Mike |
|
Energy Automation products: Sicam, Siprotec, Digsi |
|
Follow us on