(0)| 9/6/2012 12:15 PM | |
|
Joined: 1/3/2006 Last visit: 1/13/2026 Posts: 726 Rating:
|
I was trying OPC server configuration. Have two computer with name "Siemens" and "Server1". 'Siemens' is configured as OPC server, whereas Server1 is a client. OPC server is connected with 312 PLC through ISO. As shown in the <picture 4> and configurator status as in <picture 3> Problem is when from computer 'server1' I try to access the server 'OPCSimatic.NET' of computer 'siemens'error comes as shown in <picture 2>. WinCC project in "server1' shows following error <picture 1> But everthing is normal in wincc and OPC Scout of local computer (siemens) see<picture 6> and <picture 5> Thanks, Manmeet.
Attachmentss.zip (114 Downloads) |
| 9/8/2012 9:22 PM | |
|
Posts: 2661 Rating:
|
Which OPC server are you trying to use, SIMATIC NET or WinCC (OPCWinCC.Server)? |
| 9/9/2012 9:08 AM | |
|
Joined: 1/3/2006 Last visit: 1/13/2026 Posts: 726 Rating:
|
Hi Phantom75, That one is 100$ question for me, and answere is "I have no idea" !! So will ask what if difference in Simatic Net server and WinCC OPC server? InthisFAQ I found the method of configuring Simatic Net server and in some other FAQ (cannot find it now) following method was given to create WinCC OPC server
Now when to use OPC Simatic Net server and when to use WinCC OPC server, what is the difference between them and how to configure them is the question. Thanks for the time, Regards Manmeet. |
| 9/14/2012 5:47 AM | |
|
Joined: 1/3/2006 Last visit: 1/13/2026 Posts: 726 Rating:
|
|
Follow us on