(0)| 9/24/2012 8:56 PM | |
|
Joined: 6/4/2008 Last visit: 11/25/2025 Posts: 1521 Rating:
|
Unfortunately, only offline help is available in the parameter list. I have attached both the parameter list and the operating instructions for your use. Cheers, Graeme
AttachmentVC_CU2.zip (737 Downloads) |
| 9/30/2012 3:41 PM | |
|
Joined: 6/4/2008 Last visit: 11/25/2025 Posts: 1521 Rating:
|
Hi, Please see attached for the pinout for the cable, alternatively, the official cable can be ordered using part number 9ak1012-1aa00. Please doublecheck that parameters are sett as follows for full access: P051=3 P052=0 P053=7 Note: a value of 7 allows access via CB, Serial and the PMU keypad. Also, check that P927 also is set to 7, as this can be disabled. Apart from that, MOST of the parameters should be accessible. Regards, Graeme
AttachmentParameterising with Drivemonitor.pdf (722 Downloads) |
Follow us on