(0)| 10/29/2012 10:49 PM | |
|
Posts: 2 Rating:
|
Good evenening, I have written some user cycles, but most people who work on our machine are programming in ShopMill. So I decided to include my cycles in the Shop interface. It went great with standalone cycles and contours (working with the labels). Recently I discovered that it is possible to link user cycles directly in the machining plan. So I wrote a test cycle and a mask with the information given by the document. The mask works, but when i press the Softkey to generate code the mask closes but no code is generated. Not even a normal cycle block like the other user cycles do. Unfortunately I dont have the example files mentioned in the pdf, because I only program as a user on the machine. Has anyone already done something like that and could please support me? In Addition are my mask and the test cycle. Heres the link to the pdf its described in point 10.2.2 https://www.automation.siemens.com/doconweb/pdf/SINUMERIK_SINAMICS_01_2010_E/FBSPsl.pdf?HTTPS=REDIR&p=1 AttachmentE_DR_O1.zip (84 Downloads) |
Follow us on