(0)| 3/25/2011 2:07 PM | |
|
Posts: 1 Rating:
|
Hello. I'm working on the school project. We have program in Micro/Win STEP7 4.0.4.16 which operates our project. I created a simulation of a project in a WinCC Flexible 2008 SP2. I'm using a MPI cabel to communication between PC and PLC. Now i have to do a communication between WinCC and PLC which is not working ( but step7 - PLC communication works fine). Always when i try to transfer, transfer fails and it writes a error message "Info : Download is not possible. This WinCC flexible ES version and the WinCC flexible Runtime software version on the operating unit are not compatible.". Any suggestions? Our parameters are in attachment (rar file). Thx for help! AttachmentParameters.zip (131 Downloads) |
| 11/23/2012 4:26 PM | |
|
Joined: 3/2/2007 Last visit: 1/14/2026 Posts: 1002 Rating:
|
hy sirs , there are no other solutions ? thank you |
|
... thank you ... |
|
Follow us on