(0)| 12/20/2012 9:10 AM | |
|
Posts: 1121 Rating:
|
Hi If you want to upgrade your entire Plant then you will have to stop the client and Server system accordingly for the upgrade. You need not stop the AS but you will need to shut down the OS/ES. OS Client, Server. In which case your plant shall run you will lose the status and alarm that come up during that time. You will have to generate the server data, other Connections and download to AS system during which it will go to stop. End of all is that you will need a shut down of the plant. See the below links for tips on migration. LInk1 Link2 One more thing back up all the data or the user defined codes and other user defined Script as it will get replaced when u go for an upgrade. Have fun... |
Follow us on