(0)| 5/22/2007 7:35 PM | |
|
Posts: 8 Rating:
|
Hello, I'm trying to link a new WinCC aplication with an old S5 CP535. I have do it before with an S7400 an a lot of work in the data header. But now it doesnt work. I think the problem can be that in the CP535 i must configure de interface number and job number of each job, either in the local side and the remote side. This was able with Coros but not with WinCC. I have configured two links: FETCH (active at the WinCC side [SSNR 0, ANR 1]and passive at the PLC side [SSNR 0, ANR 1]) WRITE (active at the WinCC side [SSNR 0, ANR 2]and a passive RECEIVE at the PLC side [SSNR 0, ANR 2]) Is this correct?? I think its possible because ia have read it in this posts: /tf/WW/en/Posts/2072/tf/WW/en/Posts/1301 Thanks a lot!!! |
| 5/22/2007 10:12 PM | |
|
Joined: 9/1/2005 Last visit: 1/9/2026 Posts: 4114 Rating:
|
Closed: cause topic posted twice. Here you will find the second topic: WinCC CP535 in the conference SIMATIC WinCC. Best regards CS Moderator |
|
My Forum is the place to personalize your profile, |
|
Follow us on