(0)| 2/6/2013 11:18 AM | |
|
Posts: 3 Rating:
|
We have CU240E-2DP-F I don't have any errors on the drive. The drive is ready green led = on but safe led = slow blinking (STO active. I have 24V through a safety relay and back in to the drive on DI4 and DI5 but drive remains in STO. this used to work on Profisafe so could it be that I have a parameter set wrong for STO ack??? i have just raised a tech support request but it would be good if we could solve I've tried to upload the project to the thread but I don't think it has worked Thanks Colin AttachmentSimaticSinamicsSto_prob.zip (360 Downloads) |
Last edited by: O_Moderator at: 2/6/2013 2:02 PM |
|
Follow us on