(0)| 3/5/2013 6:04 PM | |
|
Posts: 53 Rating:
|
Dear expert, We are using 810D controller, Maching Centre model name: VC810. Recently after changing power module all the nc data and PLC data deleted. So I want to restore it. I have already read the procedures to reload the data from this forum. But I can't identify from siemens backup CD which one I should reload to machine. As there are too many files given by the siemens with same extensions. I have no archive in NC. So, pls help me to select the correct files from the attachment to upload it to CNC. Thanks in advance AttachmentVC-810.zip (400 Downloads) |
| 3/6/2013 4:20 PM | |
|
Posts: 53 Rating:
|
Many many thanks for your reply. Another two questions. 1. Why my files containes more than one SPF(sub program)? and which should I upload. And i didn't get any MPF(Part programm). Isn't it not necessary? 2. I have to read the PLC ladder and have to delete one line for removing one axis, as we are not using that axis. But I can't open it with s7- PLCSIM. Its saying "The selected file is unrecognised format". Anyone please check the file with others software, and inform me where the problem is? My PLC file again attached. Thanks in advance AttachmentAB0263VC.zip (311 Downloads) |
Follow us on