(0)| 3/14/2013 8:03 PM | |
|
Joined: 7/5/2007 Last visit: 1/6/2026 Posts: 77 Rating:
|
Hi Maverick05 Yes the motor can be set to run from the simodrive611, The AB servo motor is rated at 460V the infeed module can be set up to this voltage, make sure that the AB feed back encoder is a 1vpp if you need this for speed feedback, you will have to manual input all data , or using SimoComU software. Regards, Denzilg_sa Attachment611_FBU.pdf (359 Downloads) |
Follow us on