(0)| 3/30/2013 8:45 AM | |
|
Posts: 40 Rating:
|
dear sir .. i have 2 diffrent plc to run system ..which 1 was seimens s7 300 and mitshubishi Q series. using only wincc flexiable to run part of system. meaning s7 300 run by wincc flexiable,, i wantted to do new but due to limited budget of company..i had this suggestion.. where i 4 number of pc install with wincc flexiable sp3 and using pc server as well.. coonect all pc via profibus hub and connection to s7-300 and mitshubishi.. can this be done..i had try to figure it but lack of idea..attahc the drawing of what i mean to do
Attachmentkl supreme.zip (136 Downloads) |
| 4/2/2013 1:04 PM | |
|
Posts: 3037 Rating:
|
Hello ajay jay, You see which plc can you communicate with WinCC flexible in the link. SIMATIC HMI WinCC flexible 2008 Communication Part 2 Tweety |
Follow us on