(0)| 8/13/2009 7:36 AM | |
|
Joined: 5/28/2008 Last visit: 9/1/2025 Posts: 901 Rating:
|
Hello True_Blue, i not realy sure what you mean with "integrate".... you con open both project seperately and copy one device to the other projekt. regards manfred |
| 8/13/2009 8:03 AM | |
|
Posts: 217 Rating:
|
Hello, I also had the same problem and I have over come the problem by copying screens and tags (If I understand you correctly). See this past thread. Best regards, |
| 8/14/2009 5:16 AM | |
|
Joined: 10/7/2005 Last visit: 1/19/2026 Posts: 3054 Rating:
|
Hello True_Blue consider using folders in WinCCflex tosegregate the "two" projects (it will of course be one project, so this is just a cosmetic hint). See attached pic on how this could look like. Ihope this helps P.S: What advise did you get from your mentor concerning this |
|
Cheers |
|
| 4/15/2013 9:44 AM | |
|
Posts: 41 Rating:
|
I have a similar problem... I received a project from our client, and in that project every HMI panel was created from Simatic Manager. So it is, that when you open one project, you only open that panel. See screenshot 1. Before we made our own project and there each HMI panel was created inside Flexible itself. Now if you open flexible with one panel, you directly open all the panels (until the maximum of 5). See screenshot 2. In this way, you have one library with all the faceplates, one project text library,... which makes it a lot easier to work. Is there a way to move the panels into one wincc flexible project? Screenshot 1 -> screenshot 2 Thanks for all the reply. Iwein
Attachmentflexible_integrate.zip (174 Downloads) |
Follow us on