(0)| 5/11/2013 12:54 AM | |
|
Posts: 1 Rating:
|
Thank You Mr Pegaia, this was very helpful. I am working with a s7-300, I have a panel and a pc station with WinnCC RT Professional, the runtime is working properly and I am able to control a level and flow control plant with the runtime prom my pc station. However, I need to control the plant by using WebNavigator (either locally or over the internet). I setted the PC-systems's Images With Web Access for all. In the plc config I activated the web server option in the options and set the IIS (Here I have some doubts too). When I compile the project I get the followig warning: Webint: No se ha encontrado la llamada de la instrucción "WWW" (It's in Spanish because I'm from Colombia) or Webint: Instruction call "WWW" has not been found. I also says that the index.html doesn't exist. Am I suppossed to create it? Or Does the TIA PORTAL create it for me? If I have to create it, What should I do? Can you help me with some configuration to make the webnavigator work and be able to see and work with the project through internet. I have added some snapshots to show my status. Thanks in advance!!!
AttachmentProject.zip (477 Downloads) |
Last edited by: O_Moderator at: 5/14/2013 11:26 AMnew subject after splitting from /tf/WW/en/Posts/60745#top |
|
Follow us on