(0)| 5/21/2013 7:45 AM | |
|
Joined: 5/6/2008 Last visit: 1/20/2026 Posts: 25 Rating:
|
Hi, for example for the 6ES7321-7BH01-0AB0 you can find the manual here: http://support.automation.siemens.com/WW/view/en/8859629/0/ru How can you recognize if there is an existing russian variant? 1. Take the order id and put it into the search on the top on the right side. 2. Click on the order id below "product links". You will see all information on the chosen product 3.Go th the register "Entries". 4. Selectbelow "Entry types" the entry "Manuals". 5. Select the relevant manual by clicking on the blue title. 6. At the end of the entry you can see "This entry is available in the following languages:". Click on more. 7. If there is a russian manual available you can select it. If there is no russian manual available, then there is no existing translation of the manual. If you have selected "Russian", the russian manual is displayed and can be downloaded. Good luck Maulwurf |
This contribution was helpful to
|
|
Follow us on