(0)| 6/2/2013 4:59 PM | |
|
Posts: 3 Rating:
|
Hello! I need some help with configuring WinCC Flexible 2008 SP3 as OPC server. I've already read some manuals about that and have make some projects with those manuals, but i've problem with writing tag in OPC. Here some screenshots of my config: Flexible: see attachment (picture1.jpg) This is diagnostic from OPC analyser
The Core Components are installed Diagnose access to OPC server 'OPC.Siemens.XML.1' on machine 'KMW-ALC-PC'. Running on machine 'KMW-ALC-PC' as user ''KMW-ALC-PC\KMW-ALC''. The interactive user is KMW-ALC-PC\KMW-ALC DCOM is activated on machine 'KMW-ALC-PC'. Analyzer could connect to Registry on machine 'KMW-ALC-PC'. The OPC server enumerator 'C:\Windows\system32\OpcEnum.exe' has version '1.10.105'. The current version is 1.10.2 The selected OPC server type is: 'DA'. It implements the OPC Interfaces: DA1 DA2 DA3 The server description is 'OPC.Siemens.XML'. The server CLSID is '{A4A1E652-74F2-484e-AF85-3C8AC37358E1}'. The server EXE is '"C:\PROGRAM FILES\COMMON FILES\SIEMENS\OPCXML\OPCDASERVER.EXE"'. The server AppID is '{A4A1E652-74F2-484e-AF85-3C8AC37358E1}'. No AppID registry entry found for 'OPCDASERVER.EXE"'. This server has no security definitions configured. It could be that the short filename is registered. The server EXE directory '":C\PROGRAM FILES\COMMON FILES\SIEMENS\OPCXML' is not shared or not readable from user KMW-ALC-PC\KMW-ALC This is not necessarily an error. Maybe the directory is not shared or the user 'KMW-ALC-PC\KMW-ALC' doesn't have access rights. You may need to run this application on the target machine to test the file access locally. The EXE file must be accessible from the local user 'KMW-ALC-PC\KMW-ALC'. Exception at Read Registry:
OPC Scout shows this see attachment (picture2.jpg) Please told me what i should to read, or where i must put 1 instead of 0.
Attachmentpictures.zip (184 Downloads) |
Last edited by: O_Moderator at: 6/3/2013 9:02 AMpictures transferred to attachment |
|
| 6/3/2013 1:49 PM | |
|
Posts: 3037 Rating:
|
Hello, http://support.automation.siemens.com/WW/view/en/25677751 Tweety |
Last edited by: Tweety at: 6/3/2013 1:50 PM |
|
Follow us on