(1)| 6/22/2013 7:34 AM | |
|
Joined: 2/20/2010 Last visit: 10/15/2025 Posts: 104 Rating:
|
Dear Amol, You have to Asssign Make Address of CP card in your program ES configuration. In Wbe Navigator, there are Web navigator Server and Web Navigator Client is there. Web navigator client can be at any where and it's doesn't required siemens software, while in Web navigator Server is connected with either in plant bus or terminal bus as per your requirment and selection. In web Server you have to Assign your web page or Static IP addredd of your server (For static IP required only when you want to access over internet for intranet doesn't need) then you have to publish your pages(graphics) then from web client can access published page through assinged IP, here I am attachig manual for same more manual you can find from Siemens site. AttachmentWebNavigatorInformationSystem_en-US.pdf (148 Downloads) |
This contribution was helpful to
|
|
| 6/22/2013 8:02 AM | |
|
Posts: 1750 Rating:
|
You can refer this too.. Web Nevigator Step By Step I hope it will give more clarity. |
This contribution was helpful to
|
|
| 6/22/2013 8:46 AM | |
|
Posts: 52 Rating:
|
Is there any Separate document to configure Web server for 400system ,then please share. Thanks
|
| 6/24/2013 1:00 AM | |
|
Joined: 11/4/2011 Last visit: 12/24/2025 Posts: 256 Rating:
|
Hello Amol The only document on this topic that wasn't mentioned is: PCS 7 V7.0 SP1 PCS 7 OS Web option And jic PCS 7 V6.1 OS Web Option I guess you are using an older PCS7 version cause CP1613 is an older one and later was changed to CP1623. You may also take a look at one page from a Compendium Part A - Configuration Guidelines It's 7.5 PCS 7 Web option, page 242 All the other Compendiums are listed in a useful pinned topic Good Luck! |
Follow us on