(0)| 7/22/2013 10:42 PM | |
|
Posts: 2661 Rating:
|
Do you have a COM port in your PC? Check the Device Manager. |
| 7/24/2013 4:03 PM | |
|
Posts: 4 Rating:
|
Thanks for the supportPhantom75..I got the solution from customer support. Question: Facing a problem while trying to establish the communication between CPU-417 and PC with PC adapter with serial port(COM 1) . There is no local connection tab in the PC adapter(MPI) properties in set PG/PC where we can select the communication port (USB or COM).Software used .PCS7 V8.0 SP1,Windows 7 . Answer: With Windows 7 by default the PC adapter setting is USB thats why their is no choice for com ports. Users that have Windows 7 need to use the latest PC adapter USB version their is no driver for windows 7 and old PC adpapter using Comports..
|
This contribution was helpful to
|
|
Follow us on