Hi Experts....
I have a back up filewith extention .hmifor HMI MP 277. I tried to download the program to HMI through Wincc Flexible through ethernet cable to TP 277 6". I can ping the HMI with PG. But when I try to transfer the program it is giving an eror'Transfer tool can not be found'. I given the correct IP address of the HMI in the transfer settings. The HMI was in Transfer mode.Please refer the attatchments
Then I tried to download by Pack & GO option. So first I transferd the prgram to ZIP file. Then I starttransfer .BAT file following eror comes"/project/projectname/transfer/transfertool.exeis not a valid Win 32 application"
I tired with two PGS.
First PG OS is Windows XP SP3 and WinCC Flexible 2008-SP2. Second PG also Windows XP SP3 and WinCC Flexible 2008-SP2. But I didnt find 'Transfer' Option in Flexible!!!!
Please help me experts to download the program to HMI
Follow us on